Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Speed drive - Speed range ATV

Goals and Symptoms

Speed drive - Speed range
ATV

Causes and Fixes

For a speed drive, the speed range is the ratio between the output maximum frequency and the minimum frequency where the nominal torque is available.

example for a 50Hz motor :

Speed range 1/50 means the drive is able to give the nominal torque between 1Hz to 50Hz.

Speed range 1/100 means the drive is able to give the nominal torque between 0.5Hz to 50Hz.


Legacy KB System (APS) Data: RESL160729 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58