Issue
What replaces the AS-BADU-212?
Product Line
Compact
Environment
AS-BADU-212
Resolution
Component obsolescence has necessitated the AS-BADU-212 be removed from active sales. For new applications other analog input modules from the Compact line may be utilized:
For 4-20 mA and +/- 10V applications, either the AS-BADU-206 or AS-BADU-256 may be used as a replacement. (The AS-BADU-256 functions just like the AS-BADU-206 except the AS-BADU-256 operates at extended temperature).
For thermocouple and RTD applications, the AS-BADU-257 may be used as a replacement.
Đã phát hành cho:Schneider Electric Việt Nam