Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the difference between state flow and power flow?

Issue

What is the difference between state flow and power flow?

Product Line

ProWorx

Environment

ProWorx

Resolution

State flow: An instruction is select if it solves true, regardless of whether instructions "upstream" are passing power. State flow lets you see the state of each contact or coil immediately.
Power flow: An instruction only passes power (is highlighted) if it solves true and the instructions to the left of it also pass power.