Issue
The purpose of this resolution is to call attention to a QNTM module version in the ABS maritime certification listing.
Product Line
Quantum
Resolution
In the ABS Maritime Certificate of Type Approval document, Certificate Number 00-M514569-X, it is the conformal coated version Quantum Ethernet Communication module 140NOE77101C which is approved.
Đã phát hành cho: Schneider Electric Việt Nam