Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
TwidoPort 499TWD01100 Exec Upgrade to v.3.02

Issue
The purpose of this resolution is to inform TwidoPort 499TWD01100 product users that the Exec has been upgraded to version 3.02.

Twidoport modules would randomly lose their IP address or go into Kernel mode and require user intervention to become operational again. A lost IP address could be recovered by power cycling the module. To recover from a Kernel Mode failure, a Telnet login would be required to put the module into Run.


Product Line
Twidoport 499TWD01100


Resolution
Version 3.02 is more tolerant of Broadcast traffic (ARP, NetBIOS, IPX/SPX, NetBEUI) than previous Exec versions. If the tolerance levels are reached within the module. the unit will reboot without user intervention.