Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to Access a Protected Configuration in an STBNIP2212 Ethernet NIM if the Password is Lost

Issue
The purpose of this resolution is to describe how to access an Ethernet NIM Configuration if the module is password protected and the user forgets what the password is.


Product Line
STBNIP2212


Resolution
A protected configuration is inaccessible to anyone who does not know the password. The system administrator is typically responsible for keeping track of the password and the list of authorized users. If the assigned password is lost or forgotten, you will be unable to change the islands configuration. If the password is lost and you need to reconfigure the island, you will need to perform a destructive reflash of the NIM.

That is, an Exec must be re-flashed to the NIM to reset the island.