No, it doesn't support Momentum series. The ProWORX 32 I/O Drawing Generator creates CAD (Computer-Assisted Design) drawings of 800, Micro, Quantum and A120 Traffic Cop series cards. The drawings are saved in .DXF format, which is supported by most CAD programs. The ProWORX 32 Help shows detailed steps on creating, setting up and using the I/O Drawing Generator.
Đã phát hành cho: Schneider Electric Việt Nam