Goals and Symptoms
Wrong diagram in ZELIO Counts catalogue page: XBKT81030U33E.
Bad positionning of the shunt to desactivate the RESET button between 3 et 2 terminals.
Facts and Changes
XBKT81030U33E
Causes and Fixes
The right cabling is the instruction sheet diagram. The catalogue will be corrected asap. Mean while see attached file.
Attachments
(Removed File URL: 191084_4DC2/XBKT81030U33E.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/d34cde42526e5064c12573f0002bfec6/fl_block_5/0.4F0?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL191084 V1.0, Originally authored by LaBe on 02/15/2008, Last Edited by LaBe on 02/15/2008
Related ranges: Zelio Count
Đã phát hành cho: Schneider Electric Việt Nam