Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Release of STBNIP2212 RoHs Version Ethernet NIM
Issue
The purpose of this resolution is to announce that a new RoHs version STBNIP2212 Ethernet NIM was released in June 2008.


Product Line
Advantys STB
STBNIP2212


Environment


Resolution
  • What is RoHs?
    RoHs is the acronym for Restriction of Hazardous Substances. RoHS, also known as Directive 2002/95/EC, originated in the European Union and restricts the use of specific hazardous materials found in electrical and electronic PRODUCTS. The substances banned under RoHS are lead (Pb), mercury (Hg), cadmium (Cd), hexavalent chromium (CrVI), polybrominated biphenyls (PBB) and polybrominated diphenyl ethers (PBDE).
  • Identifying a NIM RoHs
    Since the part number is the same for both RoHs and non-RoHs NIMs, a RoHs compliant Ethernet NIM is identified by modules laser marked with an SV at v2.70 or higher. Non-Rohs versions will always have a firmware version less than 2.70. There are no other physical differences between the two modules.
  • Replacing a non-RoHs NIM with a RoHs NIM
    The new RoHs version STBNIP2212 is a direct replacement for the non-RoHs version. There are no functional differences between RoHs and non-Rohs NIMs.
  • Firmware
    Firmware for RoHs version NIMs will always be at 2.70 or higher. Non-RoHs NIM firmware will always be less than v.2.70.
    RoHs version firmware cannot be loaded into non-RoHs Ethernet NIMs nor can non-RoHs version firmware be loaded into RoHs Ethernet NIMs. The Exec loader file prevents the wrong version from being installed.
  • Performance
    RoHs version NIMs use an ARM9 processor instead of an ARM7 used in the non-RoHs. The faster ARM9 results in improved performance over the ARM7.