Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to find and use the PDO reference for an Advantys I/O module in a Unity application.

Issue
How to find and use the PDO reference for an 'Advantys' IO module in a 'Unity' application..

Product Line
Advantys Configuartion Software

Environment
Windows 7

Resolution
Find the 'PDO' references for the 'Advantys' IO modules using the following steps:

  • Click on the island I/O module in the 'Advantys Configuration Software'.
  • Click on 'Island\ IO Image Overview'.
  • Clcik on the tab lableled 'Fieldbus Image' in the 'IO Image Overview' window.
  • Place the cursor on one of the 'Input Data' in the table and a message will appear to describe
which input module the '6000 subindex' word applies to. (The PDO reference will be shown as
6000 with a subindex.)
dfegr


Export the 'Advantys' configuration into a '.dcf' file using the following steps:
  • Click on 'File\Export' in the 'Advantys' software window.
  • Select 'DCF' for the 'Export Format'.
  • Enter the pathname for the 'Directory' and 'Filename'.
  • Click on 'OK' to create the file.
ervgv


Import the '.dcf' file into the 'M340' configuration using the following steps:
  • Start Unity and open the M340 application.
  • Expand the 'CANopen' network in Unity.
  • Double click on the CANopen drop to open the window.
  • Double click on the 'Advantys STB island' image in the CANopen network configuration window.
  • Click on 'Channel 0' in the CANopen Network Interface Module' window.
  • Click on the 'PDO' tab to open it.
  • Right click on the 'PDO' window and select 'Import DCF' to import the dcf file.
After the '.dcf' file is imported, you will see the PDO references for the I/O modules. The references will
also be shown mapped to a '%IW' word that is shown in the 'Topo Adr' column.
egtb