Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
The substititution table for XB2B give : XB2BS8445 replaced by ZB4BS8445 But the reference ZB4BS8445t is unknown

Goals and Symptoms

The substititution table for XB2B give the reference ZB4BS8445 as substitution of the reference XB2BS8445.
But this reference is not a valid reference.

Facts and Changes

XB2BS8445
ZB4BS8445
XB4BS8445

Causes and Fixes

There must be a mistake in the cross reference files and in the commercial data base because the logical cross reference of the XB2BS8445 is the XB4BS8445.
The commercial data base has been updated in january 2010 the 11st but the cross reference list is still wrong.
This information was given to the marketing activity.