Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
When you have a power failure or when you switch off the power, the outgoing of XB5S will be have the last Status, that means, that the outgoing is in...

Goals and Symptoms

When you have a power failure or when you switch off the power, the outgoing of XB5S will be have the last Status, that means, that the outgoing is in "Switch on" Position. Is this true? It is dangerous when you have switched a function and you can't set it back after power failure. Is this known for you?

Causes and Fixes

They have a PNP or NPN transistor output. This means that when the product is not powered anymore, the transistor output will not be triggered, and the output will become or stay open, depending of its initial state.

The Biometric switch memorise the state of the output before power off. This means that when it will be powered again the output will come back to the state it was before power off.


Legacy KB System (APS) Data: RESL201136 V1.0, Originally authored by LaBe on 01/27/2010, Last Edited by LaBe on 01/27/2010
Related ranges: Harmony XB5S