Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the % voltage drop on the sinus filter both full load and other load?the data in catalog is less than 10%,not note the load,

Goals and Symptoms

What is the % voltage drop on the sinus filter both full load and other load?the data in catalog is less than 10%,not note the load,

Facts and Changes

ATV71

Causes and Fixes

About the voltage drop, the sinus filter is only a inductance the calculation is base of LWI.
L value of inductance
W value of frequency
I value of current.
10% is calculated for M3 at 100 Hz.


Legacy KB System (APS) Data: RESL202270 V1.0, Originally authored by GiVa on 05/12/2010, Last Edited by GiVa on 05/12/2010
Related ranges: Altivar 71