Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Problem with SIS Label software V3.2U

Goals and Symptoms

Problem with SIS Label software V3.2U

Facts and Changes

SISLABEL
XBY2U

Causes and Fixes

SIS Label software version 3.2U contains two malfunctions:

1/ WYSIWYG function:
When a new label model containing text is created, or when text is added to an existing model, text printing differs from its appearance on the screen.

2/ Text selection:
When text is selected in a label model it can be modified, but no information is displayed in the "character size" field. If entry of new text is required, a value must first be selected in the "size" field in order to activate the "insert text" button

To correct these two malfunctions, 5 patches have been created, each of which corresponds to an of SIS Label 3.2U (XBY2U) installation language:

Sislabel_French_01.exe
Sislabel_English_01.exe
Sislabel_German_01.exe
Sislabel_Italian_01.exe
Sislabel_Spanish_01.exe

By default the patch is installed in the SIS Label installation directory:
C:\Program Files\Schneider Electric\SISLabel

The customer can of course select an alternative installation path.

Please find below the link for patch downloading:
Sislabel_patches.zip


Legacy KB System (APS) Data: RESL202275 V1.0, Originally authored by LaBe on 05/17/2010, Last Edited by LaBe on 05/17/2010
Related ranges: Harmony XB4