How can a DIO cloud be connected to the RIO / ERIO network?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
My DIO clouds are not working when they are attached as part of the RIO / ERIO network, How can a DIO cloud be added?

Product Line:
M580
Quantum

Environment:
Unity Pro
EcoStruxure Control Expert

Resolution:
There are 3 ways DIO clouds can be connected to the RIO / ERIO network.

1.) Connect the DIO cloud to the Service Port on the M580 CPU module or CRA module.
2.) Connect to any port on a NOC or NOS module.
3.) Connect to the specified port on the Connexium Managed switch using the pre-built configuration files.

Refer to the attached manuals for further information.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Phần đính kèm
Modicon M580 Standalone System Planning Guide.pdf [16.22 MB]
Modicon M580 System Planning Guide for Complex Topologies.pdf [3.44 MB]
Modicon M580 Hot Standby System Planning Guide Frequently Used Architectures 2017.pdf [14.12 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: