Product Line
CM4000
CM4250
CM4000T
Resolution
The maximum number of Digital Inputs available on a CM4000 is 16.
Eight digital inputs are available on the I/O Extender via the IOX08 option and digital inputs are available with the digital I/O option card IOC44.
Đã phát hành cho: Schneider Electric Việt Nam