Issue
User would like to know what the Distortion Power Factor is and how the value is calculated
Product Line
CM4000
Environment
ION Setup
CM4000 Logs
Cause
Distortion Power Factor is an unknown calculation for the CM4000 meter.
Resolution
Distortion power factor is a percentage measured by the CM4000. It is calculated by dividing the Overall Power Power Factor by the Fundamental Power Power Factor.
For more information please refer to the CM4000 Reference Manual attachedWhere to find documentation for the CM4000 series meter? | Schneider Electric USA
Đã phát hành cho: Schneider Electric Việt Nam

Discontinued

Discontinued