Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Clients that connect to the primary alarm server while it is resyncing do not get alarm data

Goals and Symptoms

Summary:
Clients that connect to the primary alarm server while it is resyncing do not get alarm data.
The listener on the alarm server is opened before the alarm server is ready (resynched)

Causes and Fixes

Summary:
Clients that connect to the primary alarm server while it is resyncing do not get alarm data.
The listener on the alarm server is opened before the alarm server is ready (resynched)


Solution:
The listener on the alarm server is now not opened before the alarm server is ready (resynched)