Issue
There is no good way to reset Peak Demand on the PM800 series (or other Powerlogic Devices)
Product Line
ION Enterprise or SPM7, PM800
Environment
VIP
Resolution
The attached process will reset the Power Min/Max Demand at the start of every month, based on when the 'Clock' determines that a new month has began--not '30 days elapsed'.
This process can be used for other values that should be reset at the start of every month as well, so long as it is a value that the register is accessible via ION Enterprise.
Please check the attachments to download instruction file: 'Clock-Based_Reset_Instructions'.
Đã phát hành cho: Schneider Electric Việt Nam