Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What firmware level do I need to have in the CM4000 to view the Energy Usage ECC web page?
Issue
Older versions of the firmware do not support the trending values.

Product Line
CM4000

Environment
Web Applications
Firmware

Resolution
The trending values for this feature are not activated in older firmware versions.
The CM4000 firmware will require upgrading to version 12.100 or greater.

Access to firmware upgrade instructions, including a how-to video and a link to the latest firmware can
be found at: Firmware Upgrade - Instructions and Downloads

Additionally, supporting documents and file downloads on this and a wide variety of other products and topics may be
obtained using the search function found at the: Download Center