Hôm nay chúng tôi có thể giúp gì cho bạn?

Which fuses are used with the Enercept Meter and the Energy Meter Fuse pack?

Issue
Would like to know fuse class for fuses included in the energy meter fuse packs

Product Line
EMFP1
EMFP2
EMFP3

Environment
Installation

Resolution
The replacement fuses for the voltage fuse pack with the Enercept Meter or Energy Meter are 1/2 AMP Cooper, Bussmann, FNQ-R-1/2, CC-Tron, Class CC, Slow Blow.