Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
WebReach can display real-time data but can't display Objects

WebReach can not display objects, however real time data can be displayed. The possible cause might be a missing dll file called ImgX61.dll which runs under WebReach engine to display objects. It can be located on the install disc. Copy the file into .../ION Enterprise /system/bin and register it:
1. Open a CMD prompt and navigate to .../ION Enterprise/system/bin
2. Register imgx61.dll by typing:

regsvr32 imgx61.dll

3. Exit the CMD prompt




Last Revised: November 13, 2007
Applies To: WebReach
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189170 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5