Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can I retro-fit my 73xx series from a normal display to a RMD?

The meter would require full retro-fit (RMA) of all boards to change over to an RMD, this would require the meter to come back to the factory. Contact RMA for details & cost. It is likely more effective for the customer to exchange the meter if it is still un-opened or to keep this meter and buy a Tran/RMD model as well if the display model was previously installed.

Last Revised: November 19, 2007
Applies To: ION 7300/7330/7350
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189305 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION7300