Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why is the Time Sync Count not increasing?

In each ION Meter, the Diagnostic module has a "Time Sync Count" output register. This register indicates how many time-synchronization signals have been received. The value increases with each signal received. In some cases, this register is not increasing, although it is obvious the meter has been re-synchronized.

This is most likely because the synchronization type is set to NTP (Network Time Protocol). Using the ION synchronization, ION Enterprise detects that the meter if off-sync, and will send a sync signal.
When using NTP, the meter ignores the sync signals coming from ION Enterprise. With this setting, the meter doesn't actually RECEIVE a synchronization signal, as it will synchronize by itself on a network clock. That's why the time sync counter doesn't increase when NTP is selected.