Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to link to a module's setup registers in ION Enterprise Designer.

In order to link an input of a module to a setup register of another module in Designer first choose the input that you would like to link to a setup register. Next, hold down Ctrl and left click on the output of the module that you need to connect to a setup register of. Choose a setup register and the task is completed.

Date Created: July 22, 2009
Last Revised: July 22, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199435 V1.0, Originally authored by MiNe on 07/23/2009, Last Edited by MiNe on 07/23/2009
Related ranges: ION Enterprise V5.5, ION Enterprise V5.6