Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to determine the details of hardware key licenses for Powerlogic SCADA, specifically web client licenses?

Each Powerlogic SCADA (PLS) hardware key is individually programmed to contain a specific number of licenses. In order to view the license information for a specific key:
-Open Powerlogic SCADA Explorer
-In the Citect Explorer window, click on Help and select Citect Key Update



-The details of the key are listed in the window. The number of control and view-only are listed next to Web/Internet Controls Clients and Web/Internet View-only Clients, respectively.



The CiUSAFE application that displays the details of the key can also be launched from the following location:
C:\Program Files\Schneider Electric\PowerLogic SCADA 7.10\Bin\CiUSAFE.exe\

Key Words and Phrases: Site ID, SiteID, site identification

Document Change History

Date and InitialsComments
2010-11-04 DRM* Add key words and phrases upon suggestion of LF

Legacy KB System (APS) Data: RESL200005 V3.0, Originally authored by KBAdPM on 09/19/2009, Last Edited by DaMi on 11/11/2010
Related ranges: PowerLogic SCADA 7.1