Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why is the menu definition not visible in PowerLogic SCADA Web client

Issue
The menu definition is not visible for project in web client.


Product Line
PowerLogic Scada 7.x

Environment
Webclient

Cause
The menu.dbf file is not being zipped up correctly during client web deployment.

Resolution
Follow the procedure below.

1. Go to your project folder (eg. C:\Documents and Settings\All Users\Application Data\Schneider Electric\PowerLogic SCADA 7.10\User\EMG)

2. Zip 'menu.dbf' file and name it as 'misc.zip' as per below.


3. Go to Citect Explorer -> Try 'Web Deployment Preparation' again.


4. Try Web Deployment again under your Internet Explorer and restart your Webclient.


5. Then you can see your menu definition as per below.