Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
ION Enterprise 6.0 - controlling of access to reports created web reporter - sharing access and restricting to certain groups or individuals

Goals and Symptoms

Is it possible to give access to a report only to specific users?
For example, let's say customer A should see report A but not report B and, similarly, customer B should see report B but not report A.

Causes and Fixes

It can be done by go to webreporter; login and then go to File > Manage > Share.


Here, the "share list" for each report can be defined to control who has access to which report.

NOTE; These properties can only be set by a user of an account with "supervisor" level privileges (i.e. operator, controller, user nor observer have permission to modify this report share function)


Legacy KB System (APS) Data: RESL201530 V1.0, Originally authored by KBAdPM on 03/03/2010, Last Edited by KBAdPM on 03/03/2010
Related ranges: ION Enterprise V6.0