Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is Clearance for Mounting PM7?

Issue

What is the clearance for mounting PM7?

Product Line

PowerLogic PM700 Series

Environment

PM700 Series Energy Meters – Installation Requirements

Resolution

The clearance for mounting a PM7 meter is the same as the clearance for mounting a PM8 meter.

Please refer to the following diagram for installation reference:

1


1
Last Revised: 14 May 2010
Original Author: EF
Public
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL202583 V1.0, Originally authored by KBAdPM on 06/12/2010, Last Edited by KBAdPM on 06/12/2010
Related ranges: PM700 series