Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
ION Enterprise V6.0 SQL Server 2005 Express installation error: "Error 1706. Setup cannot find the required files. Check your connection to the network, or CD-ROM drive. For other potential solutions to this problem, see c:\Program Files\Microsoft Office

Goals and Symptoms

This error message appears after clicking Upgrade SQL Server Express on the ION Enterprise V6.0 installation menu:


Error message text:

Microsoft SQL Server 2005 Setup

Error 1706. Setup cannot find the required files. Check your connection to the network, or CD-ROM drive. For other potential solutions to this problem, see c:\Program Files\Microsoft Office\OFFICE11\1033\SETUP.CHM

Causes and Fixes

There are 2 solutions to this issue.

Solution 1:
Uninstall SQL Server 2005 Express completely and then try to manually run the OWC11.msi file available in the Tools folder of SQL Server 2005. After this, install SQL Server 2005 Express again.

Solution 2:
Uninstall Office Web Components from Add/Remove Programs in the Control Panel. After this, upgrade SQL Server 2005 Express again.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/49cec399bdc3f830c125774500109d86/fl_block_5/0.1A60?OpenElement&FieldElemFormat=gif)
Date Created: June 11, 2010
Last Revised: June 16, 2010
Public
Original Author: MN
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL202644 V1.0, Originally authored by LaAd on 06/17/2010, Last Edited by LaAd on 06/17/2010
Related ranges: ION Enterprise V6.0