Issue
The purpose of this resolution is to provide instructions on how to create a customized toolbar and add icons
to the new customized toolbar in ProWORX 32,
ProWORX 32
Environment
Windows 7, 10
Resolution
The following procedure can be used to create a new customized toolbar inProWORX 32.
- Right click on the toolbar and select customize.
- Click on the 'New' button.
- Type in a name for the new toolbar.
- Click on the 'OK' button
- Closeout the 'Customize' window by clicking on the 'Close' button..
- Drag the new toolbar icon and reposition it on the menu bar space.
- Right click on the added toolbar icon and select customize.
- Click on the 'Commands' tab
- Click on an item in the 'Categories' list.
- Click on the icon in the 'Commands window and drag the icon over to the new toolbar.
- The following figure shows the icon added to the new toolbar.
Đã phát hành cho:Schneider Electric Việt Nam