Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do I configure the Vijeo Designer Runtime on an iPC to use the Windows windows controls

For an iPC target, there is a "Windows Control" group of properties at the target level in Vijeo-Designer.
-Disable Key Control:
When set to "Disabled", the "key control" is available. This means that special combinations of keys from Windows are available (e.g. Alt+Tab to switch between applications, Alt+F4 to close an application, access to the Windows key).
When set to "Enabled", the "key control" is unavailable. This means that there is no way to switch from Vijeo-Designer Runtime to another Windows application.

Property Inspector


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)