Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
ION7650: 10Base-T or 100Base-TX communication card?

Issue

Networking hardware used for an ION7650?

Product Line
ION7650

Environment
Communication

Cause

The ION7650 doesn't have Ethernet capability.


Resolution
With the release of the v350 firmware, the ION7650 was equipped with a new Ethernet card capable of 10BASE-T / 100BASE-TX, compared to 10BASE-T in the previous versions. This is done to ensure compatibility with high speed networks. This has no effect on the communication speed of the device itself as the limitation is coming from the CPU board and not from the card. All new meters ordered after January 1, 2008 will include the new communication card.

Meters including 10BASE-FL Fiber option (order number "F0" and "D1") will include a 10BASE-T Ethernet card only.
Meters with the 100BASE-FX option (order numbers "F1" and "D7") include a 100BASE-TX Ethernet.