Issue:
Setting up Ethernet TCP/IP on the ATV61 and ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Ethernet TCPIP manual VW3A3310D
Resolution:
You can find ethernet configuration assistance in the ATV61/71 Ethernet TCPIP manual 30072-452-37
Đã phát hành cho: Schneider Electric Việt Nam