Issue:
Need to adjust the Scale Factor for the Voltmeter, Ammeter, or Wattmeter values of a Power Meter 800.
Product Line:
Powerlogic PM800 Series Meter
Cause:
Customer wants to adjust the Scale Factors used for the Voltmeter, Ammeter, or Wattmeter Values of a Power Meter 800.
Resolution
See attached document.
(How_to_adjust_the_scale_factors_used_for_the_Voltmeter,_Ammeter,_or_Wattmeter_values_of_a_Power_Meter_800)
Đã phát hành cho: Schneider Electric Việt Nam