The Steel sheet metal thickness used in Okken switchboard is as listed below:
Okken Steel sheet metal thickness
Okken Steel sheet metal thickness
| Housing | Thickness mm |
| Door | 2.00mm |
| Rear panels | 1.50mm |
| Side panels | 1.50mm |
| Roof | 1.50mm |
| Inter Cubicle | 1.50mm |
Đã phát hành cho: Schneider Electric Việt Nam