Issue:
What is the difference between the Basic Shunt Trip and Full-Featured Shunt Trip versions of the Enclosed ATS22?
Product Line:
Enclosed AST22
Environment:
All models
Cause:
Define features for quoting
Resolution:
The electrical schematics are the same. The Basic Shunt Trip unit is a space optimized version of the Enclosed 22 controller. Limited space is provided for field mountable control equipment. The Full-Featured Shunt Trip unit is a fully customizable version. Additional space is provided for engineered options and field installable equipment.
Đã phát hành cho: Schneider Electric Việt Nam