Issue:
Wondering if the VW3A8120 simple loader tool, work on the ATV212 drives?
Product Line:
VW3A8120
Environment:
All serial numbers for VW3A8120
Cause:
Range of compatibility
Resolution:
The simple loader VW3A8120 is currently not compatible with the ATV212 drive.
The Range compatibility
ATV12
ATV312
ATV61
ATV71
ATV32
ATV31C
ATV Lift
ATV61Q
ATV71Q
Đã phát hành cho: Schneider Electric Việt Nam