Issue:
How do you change IP rating on the ATV61 drives?
Product Line:
Altivar 61 ATV61
Environment:
All
Resolution:
The open style ATV61H... part number is on the nameplate and in the drive menu 1.11 Identification.
When the Power Identification (Prt) is changed from IP20 to IP00, the VFD rating increases up one size and the part number changes from ATV61H to ATV61K.
The IP rating change is only done in our enclosed packages by Schneider Electric after passing Standard testing. The IP change should never be done on open-style drives.
To check the Power ID or to change it:
1. Navigate to menu 2 [ACCESS LEVEL]. Set to [Expert].
2.In menu 1.4 [MOTOR CONTROL], find parameter Power Ident (Prt)
Setting options are IP00 and IP20
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Đã phát hành cho: Schneider Electric Việt Nam