Issue:
Err7 Fault ATV212.
Product Line:
ATV212
Environment:
All serial numbers for ATV212
Cause:
N/A
Resolution:
Err7 means the motor current sensor in the drive is inoperable. The best resolution would be to replace the drive.
Đã phát hành cho: Schneider Electric Việt Nam