Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why do I see 115 VAC on the outputs of the BMXDAO1605 when there is no load connected to to module?

Issue:

Why do I see 115 VAC on the outputs of the BMXDAO1605 when there is no load connected to to module?

Product Line:

BMXDAO1605

Resolution:

This is normal when attempting to measure a triac output with no load.  Triac outputs cannot be accurately tested without a load.
The high impedance of the voltmeter will introduce enough of a load to cause the applied voltage on the triac to be seen.
Test with a load applied to the triac and you'll get a more meaningful measurement.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)