Issue:
Is a remote keypad come with the ATV312 drive as standard?
Product Line:
ATV312
Environment:
All models and serial numbers
Cause:
None
Resolution:
The ATV312 drive does not come with a remote keypad as a standard item. It must be ordered separately.
Remote Keypad Display
(IP54) ATV312, ATV12 VW3A1006
(IP65) ATV312, ATV12 VW3A1007
Mounting Kit, VW3A31101
Graphic Display (used also with ATV61 and ATV71) VW3A1101
Đã phát hành cho: Schneider Electric Việt Nam