Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
In Control Expert, how do I add the Ethernet and Remote IO Drops to a Quantum CPU application?
Issue:
In Unity Pro, how do I add the 140CRA31200 to a rack?

Product Line:
Unity Pro, 140CRA31200

Resolution:
To enable Ethernet RIO you must add a 140CRP31200 to the local rack.  There will be another node below the Local Quantum Drop called EIO bus.    Open the EIO bus, <double-click> on the drop (square box) and select your slot size.  Once that is complete, you will see the Quantum slot rack with a 140CRA31200.

To enable S908 RIO you must add a 140CRP93x00 to the local rack.  There will be another node below the Local Quantum Drop called RIO bus.    Open the RIO bus, <double-click> on the drop (square box) and select your slot size.  Once that is complete, you will see the Quantum slot rack with a 140CRA93100.