Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can a SoMachine v4.x installation co-exist on a PC that has other versions of CoDeSys software installed?
Issue:
Can a SoMachine v4.x installation co-exist on a PC that has other versions of CoDeSys software installed?

Product Line:
SoMachine, CoDeSys

Environment:
PLC Configuration Software for Windows

Resolution:
In general, the parallel installation of CoDeSys-based software and SoMachine V4.x should not have any issues.
One known issue is the Gateway but the Gateway Management Console of V4.x allows to switch between all available gateways.
In the General Tab of the Gateway Management Console, press the "Switch Gateway Service" button to select a Gateway Service from those that are installed on the PC.