Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Where can I find customer factory wiring diagrams for M-Flex and MCC enclosed custom built drives and soft starters?

Issue:
Looking for factory wiring diagrams for M-Flex and MCC enclosed custom built drives and soft starters.

Product Line:
Altivar ATV61, 71 M-flex enclosed MCC units

Environment:
All

Cause:
Needs factory wiring diagrams for a custom enclosed drive.

Resolution:
You will need to have the factory order number (FO), wiring diagram number (WD), or the drawing number.

Once you have the factory order number you can contact the Drives Product Support Group at 1888 -778-2733 choose option 2 and then option 4.

You can also reach out using the Chat option on the Schneider Electric webpage or by emailing to drive.products.support@se.com.

The Drives Product Support Group will pull the drawings from the data base and email them to you.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)