Hôm nay chúng tôi có thể giúp gì cho bạn?

How to Time Sync a PM800 Meter from ION Setup?

Issue
Interesting in syncing the clock on the PM800 meter to get more time-accurate readings.
Product Line
PowerLogic Meters
PM800 Meter
Environment
ION Setup v 3.x
Ethernet enabled PowerLogic Devices
Resolution
  1. Start up the ION Setup program and entering the proper credentials (default supervisor account password 0). NOTE: Make sure the box for "Single ION device configuration mode" is unchecked.
ion setup login screen
  1. Add the device if not added already. You can do so by following this process: How to add a device into ION Setup | Schneider Electric USA
  2. Once the device is added to ION Setup and is connected to by the user the following list of configuration options will show up on the right-hand side. Click on the clock option to open the clock settings.
configuration options for powerlogic meter
  1. Within the clock options, you can check the boxes of the different clock setting you would like to update. Once you have selected the associated boxes, you can press 'Send' at the bottom to sync the clock of the meter.
clock settings for the meter