Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is there a way to automatically logout of an Magelis/Harmony HMI after a time interval of inactivity?
Issue:
Is there a way to automatically logout of an Magelis/Harmony HMI after a time interval of inactivity?

Product Line:
Magelis XBTGC/GK/GT, Harmony HMIGTO/STO/STU, Magelis Smart iPC, Magelis Compact iPC, Magelis Flex Box, Magelis Smart Box, Magelis Compact Box, Harmony Panel PC, Harmony Box PC, Harmony P6, Vijeo Designer

Environment:
Vijeo Designer Runtime on HMI

Resolution:
Yes, you can set the Magelis/Harmony HMI to log out after an inactivity time.  That setting is in the Security Properties under Inactivity Time-out of the Logout Behavior.

Please see below screenshot for more information.

Vijeo Designer Buildtime Project Navigator > Environment > Security settings

The value of the Inactivity Time-Out is in minutes.  When downloading to the target, you will need to check the box to delete the "preserve runtime data" to update the security settings.