Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Created a Vijeo Designer project within SoMachine v4.1, v4.2 or v4.3, why is the simulation button greyed out?
Issue:
Created a Vijeo Designer project within SoMachine v4.1, v4.2 or v4.3, why is the simulation button greyed out?

Product Line:
Vijeo Designer, SoMachine

Resolution:
If you have installed SoMachine v4.1, v4.2 or v4.3 (which includes an embedded version of Vijeo Designer v6.2), but only registered the license for SoMachine, when creating a Vijeo Designer project outside of SoMachine (as "Standalone" Vijeo Designer), you will not have an option to run the Simulation mode.  In order to run Simulation mode, you will need a stand alone license for Vijeo Designer.

One easy solution for this is to archive the Vijeo Designer project as .VDZ and import it into SoMachine. When opened inside a registered SoMachine, Simulation mode will be available.