Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is there a touchscreen type HMI available for the ATV61/ATV71 series drives?
Issue:
Is there a touchscreen type HMI available for the ATV61/ATV71 series drives?

Product Line:
Altivar

Environment:
Altivar Machine

Cause:
Customer is searching for a "touchscreen" type HMI to connect to the ATV61 / ATV71 series drive.

Resolution:
There is no "plug and play" touchscreen HMI available for the ATV61 / ATV71 series drive.   There are many Magelis touchscreen HMI that can be used with the ATV61 / ATV71 series drives, but they will need to be programmed to connect to the drive via a Modbus RTU port and will also have to be programmed to access the desired parameters within the drive.   It will not be pre-programmed to access the drive menus, but through proper programming of the HMI, it can be used to interface with an ATV61 / ATV71 series drive for full control or monitoring only.