Issue:
Rail mounting kit availability for an ATV212HD15N4.
Product Line:
ATV212, Altivar 212 Altivar buildings
Environment:
Altivar 212H075M3X...U22M3X
Altivar 212H075N4...U22N4
Cause:
Din rail mounting inside a panel.
Resolution:
There is no DIN rail mounting kit for the ATV212HD15N4.
The DIN rail mounting kit part number VW3A31852 isfor installation on 35 mm wide DIN rail that are available only for: Altivar 212H075M3X...U22M3X and Altivar 212H075N4...U22N4, the smaller HP sized drives.
Đã phát hành cho: Schneider Electric Việt Nam